Other Parts Discussed in Thread: CDCE913
Hi,
I am using CDCE913 in my design to generate different frequencies via I2C Control.
I was reading the datasheet (Section 8.3.4) for determining the slave address of the device to control it via I2C and it states the following:
"Address bits A0 and A1 are programmable through the SDA/SCL bus (byte 01, bits [1:0]. This allows addressing up to 4 devices connected to the same SDA/SCL bus. The least-significant bit of the address byte designates a write or read operation. "
My question is, the I2C slave address is programmable via I2C (SDA/SCL) bus but don't I already need a slave address to begin any I2C communication.
In other words, is there a default slave address on the CDCE913 device that I can use to start I2C communication and then configure the A0 and A1 bits to assign new address if required?
Thanks
Amninder