This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04906 - PLL2 settings

Other Parts Discussed in Thread: LMK04906

Hello,

We are having trouble translating settings for PLL2 from the LMK04906 evaluation board to our circuit. We are using the part in dual loop mode with a 40 MHz VCTCXO as the VCXO for PLL1.

We have populated the 40 MHz VCTCXO on the LMK04906 evaluation board and the performance is satisfactory with PLL2_C4_LF set to 146 pF. However, when we try to use these settings on our board, which is electrically identical, PLL2 is unstable and does not lock. Adjusting the charge pump current has no effect.

Your assistance is appreciated!

Best Regards,

-Bud