Hi,
I'm using the LMK03806 as multiple clock source. For this application it's important to make use of the "SYNC" input in order to start multiple clocks with defined phase relation. According to the data sheet this is very simple: when SYNC is asserted, all sync-selected output clocks go low, after de-assertion they start with defined phase relation.
In fact this doesn't seem to work at all: whatever clock is selected to be SYNC'd (by setting the appropriate NO_SYNC_CLKout bit to zero) is just "dead" all the time - no matter which level or edge is applied to the SYNC input. The only way to get my clocks working is to disable the SYNC (by setting the appropriate NO_SYNC_CLKout bit to one) - the I get the clock signals, but they are not in defined phase-relation.
Why doesn't the SYNC seem to work - what I'm doing wrong here ????
Thank's a lot,
Markus