On the TDC7200, range in mode 2 is up to 8ms.
Does that depend on the clock frequency?
If I use a 16MHz clock, what is the max time period to be measured?
With a 16MHz clock, can it send new start pulses at a rate of 1kHz?
What determines the max rate at which new start pulses can be sent?