Just downloaded the new Clock Designer which includes LMX2571. It seems that in the Loop Filter Select dropdown, your only options are 0 Hz, Inf Hz, 4th Order and Brickwall. It would be nice to have 2nd and 3rd Order as well. In the LMX2571 Ext VCO option, these options are present but not for the Internal VCO config. I suppose I can use the Ext VCO option with a VCO similar to the internal VCO and I should get similar results. Anyone see any problems with this workaround? Thanks
Bob