This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK4201 corrupted signal

Hi All,

I have a design with the following link:

Virtex 2 Pro Rocket IO (Aurora TX ) => Loopback => 5.6nF AC coupling => TLK4201 => 5.6nF AC coupling => Virtex 2 Pro (Aurora RX)

You can see the  signal at the input of the TLK4201 at: http://imageshack.com/a/img538/6388/WdBxuT.png

You can see the signal at the output of the TLK4201 at : http://imageshack.com/a/img661/1295/JozPgA.png


I can't understand why the signal gets so corrupted after going through the equalizer

Any one have an idea?

Thanks