Hi,
Regarding Dual Loop Mode setting for LMK04826,
In Dual Loop Mode as shown the datasheet Figure15, we have confirmed that PLL2 has achieved lock.
However, in Cascaded 0-delay Dual Loop Mode as shown the datasheet Figure16, the PLL2 couldn't be lock.
The evaluation condition is as follows, and I have attached the dump list.
・CLKin0 = 122.88MHz
・OSCin = 30.72MHz
・Phase Detect(PLL1) = 7.68MHz
・Phase Detect(PLL2) = 30.72MHz
・VCO = 1966.08MHz
・DCLKout0 = 122.88MHz
・DCLKout6 = 983.04MHz
・Address 0x13F = 0x11
・Address 0x140 = 0x00
・Address 0x147 = 0x0A
・Address 0x138 = 0x00
Please let me know if the settings are wrong.
Best Regards,
Kato
0x0000 0x80 0x0000 0x10 0x0002 0x00 0x0100 0x30 0x0101 0xAA 0x0103 0x01 0x0104 0x2A 0x0105 0x00 0x0106 0x70 0x0107 0x11 0x0108 0x30 0x0109 0xAA 0x010B 0x01 0x010C 0x00 0x010D 0x00 0x010E 0xF8 0x010F 0x00 0x0110 0x22 0x0111 0xAA 0x0113 0x01 0x0114 0x2F 0x0115 0x00 0x0116 0x70 0x0117 0x55 0x0118 0x22 0x0119 0xAA 0x011B 0x01 0x011C 0x2F 0x011D 0x00 0x011E 0x70 0x011F 0x55 0x0120 0x22 0x0121 0xAA 0x0123 0x01 0x0124 0x2F 0x0125 0x00 0x0126 0x70 0x0127 0x55 0x0128 0x30 0x0129 0xAA 0x012B 0x01 0x012C 0x00 0x012D 0x00 0x012E 0xF0 0x012F 0x01 0x0130 0x22 0x0131 0xAA 0x0133 0x01 0x0134 0x2F 0x0135 0x00 0x0136 0x70 0x0137 0x55 0x0138 0x00 0x0139 0x00 0x013A 0x02 0x013B 0x00 0x013C 0x00 0x013D 0x11 0x013E 0x00 0x013F 0x00 0x0140 0x00 0x0141 0xFF 0x0142 0x00 0x0143 0x91 0x0144 0x00 0x0145 0x7F 0x0146 0x02 0x0147 0x0A 0x0148 0x02 0x0149 0x42 0x014A 0x00 0x014B 0x0E 0x014C 0x36 0x014D 0x00 0x014E 0xC0 0x014F 0x7F 0x0150 0x03 0x0151 0x02 0x0152 0x00 0x0153 0x00 0x0154 0x10 0x0155 0x00 0x0156 0x10 0x0157 0x00 0x0158 0x96 0x0159 0x00 0x015A 0x04 0x015B 0xD4 0x015C 0x20 0x015D 0x00 0x015E 0x00 0x015F 0x1E 0x0160 0x00 0x0161 0x01 0x0162 0x40 0x0163 0x00 0x0164 0x00 0x0165 0x0A 0x017C 0x18 0x017D 0x77 0x0166 0x00 0x0167 0x00 0x0168 0x20 0x0169 0x59 0x016A 0x20 0x016B 0x00 0x016C 0x00 0x016D 0x00 0x016E 0x3E 0x0173 0x00 0x1FFD 0x00 0x1FFE 0x00 0x1FFF 0x53 0x0143 0xB1 0x0143 0x91 0x0144 0xFF 0x0143 0x11 0x0143 0x10 0x0139 0x02 0x0139 0x03