This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lmx2541

Other Parts Discussed in Thread: LMX2541, LMX2581, LMX2571

Hello, my name is Nick, i choose de lmx2541 to make spectrum measures and i need to generate a lot of diferent frequencies sequentially in the band of 100Mhz to 200Mhz,  my question is this is the right c.i to do so?what cares do i have to consider in the pcb and program? i read the datasheet but i can't decide because there are also others lmx and i want to make sure that the lmx2541 is suitable for this application.. thanks!

  • Hi Nicolas,
    LMX2541, LMX2581 and LMX2571 can support your application. Selection between them depends on your application and performance requirement. For example, if you need lower current consumption, select LMX2571. If phase noise is more important, select LMX2541 or LMX2581. If you could provide us more information on how you will use the device, we can make a suggestion to you.