This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828B PLL operation without External VCXO

Other Parts Discussed in Thread: LMK04828

Hi,

I plannind to use LMK04828B PLL in my module. As per the architecture of LMK04828 chip there are two stage PLL & PLL1 CP_out has been used for controlling a external VCXO & the VCXO out shall be given to the Oscillator input as the input of the second stage PLL.


Is there any option(Other than External VCO input), in which without using the VCXO, PLL VCO frequency can be generated.

Regards

Soumya S