This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Clock bias and amplitude adjustment

I am looking for a solution to the following:

An LVDS pulse is provided by an FPGA that is 200MHz (5 ns).  A DAC is providing two inputs that are a DC bias 0-5V and an amplitude adjustment also 0-5 V.  The circuit would allow amplitude adjustment of the FPGA clock and a DC  bias adjustment of the FPGA clock without changing the pulse width (5 ns).  The output of this circuit would be 0-1V.  As the DAC is changed the output pulse would reflect the adjustment.

Thanks,

Earl