Hi: I purchased the evaluation kit for the LMX2571, and I am trying to get it working. I have the ANYUSB interface updated and it is working. Also, the port setup is completed and working. I would like some assistance to get to "first base" with the device, that is to use it to generate a signal and see the PLL lock light come on. I would like to use the 20 MHz on-board oscillator, and synthesize a 100 MHz signal using PLL F1 and a 150 MHz signal using PLL F2. F1 could come out on RFout TX and F2 could come out on RFout Rx. This would be a good example, to get things going. On the dashboard, it indicates that PLL F1 is active and PLL F2 is not active, and is operating with External charge pump. I would like to activate both PLLs, for the frequencies indicated, Can you advise the register settings to achieve this ? The best thing, I think, is if someone could email me a settings.mac file, that I can load,for the frequencies indicated, and that should do it . Any assistance would be greatly appreciated,
Doug Maenpaa
Accutron Instrumentsd Inc