Hi All,
I have absolutely no experience in clock generation so I was wondering whether the following can be achieved (and what would be the best way to do so):
- Would it be possible to generate a 180MHz, low output jitter, LVDS clock signal from a single common value (8-32MHz) crystal oscillator?
- What would be the best starting point for such a solution?
- This will be for experimental purposes, so there is no limitation on the part count / cost.
- Can the above LVDS output be further improved by running it through a clock jitter cleaner?
- Is such a solution possible without a digital interface to the clock generator (i.e. can the output frequency / dividers be set using external passive components?)
This clock source will be used for a high speed DAC.
Any feedback would be greatly appreciated.
Regards
Marius