What is the frequency lock time for the LMX2492?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
David,
The lock time is almost completely governed by the loop bandwidth of the loop filter, which is set by external components. Making a wider loop bandwidth speeds lock time, but degrades phase and spurs.
If one was to disregard phase noise and spurs, you can design a very widebandwidth filter to lock in a few us, but you probably would decide that you do care somewhat about phase noise and spurs and then this becomes a few 100 uS.
For the ramping features, we have done a 10 us ramp with a 500 kHz loop bandwidth and the spurs/phase noise were not too bad. But in the case of ramping, the PLL doesn't have to fully lock, so this is why these times are pretty fast.
Regards,
Dean