Other Parts Discussed in Thread: LMK04803, CODELOADER
Hi,
We have the following issue with the LMK04803 clock-jitter-cleaner.
We use the chip according to the attached schematic (pdf).
Our problem is, the the PLL does not lock in 0-delay mode - we did not try non-0-delay.
First we experienced the issue with the "2nd stage" (U101), the first IC (U100) was in clock-distribution mode.
In this case there was rarely lock - for U101 -, but only after power-reset, never after soft-reset.
Then programming the first (U100) IC to "dual PLL w 0-delay" mode there was no lock at all.
U101 programming would start after U100 lock, but never happened.
I also attached the configuration files.
What could be the problem?
Another remark:
I used Codeloader for register value checking.
The program does not take in account 0-delay mode for feedback path divider calculation.
Thanks,
Greg
R0 (INIT) 0x80160100 R0 0x00140100 R1 0x00140101 R2 0x00140102 R3 0x80140103 R4 0x00140104 R5 0x80140105 R6 0x11110006 R7 0x00110007 R8 0x00110008 R9 0x55555549 R10 0x10005D0A R11 0x1400200B R12 0x1B0C006C R13 0x0303824D R14 0x0300000E R15 0x0000800F R16 0x41550410 R24 0x00000058 R25 0x01010019 R26 0xAFA8001A R27 0x1C00009B R28 0x0020009C R29 0x0100005D R30 0x0100005E
R0 (INIT) 0x80160100 R0 0x00140140 R1 0x00140141 R2 0x00140142 R3 0x80140143 R4 0x00140144 R5 0x00140145 R6 0x11110006 R7 0x00110007 R8 0x11110008 R9 0x55555549 R10 0x10005C0A R11 0x4400200B R12 0x130C006C R13 0x0303800D R14 0x0300000E R15 0x0000800F R16 0x01550410 R24 0x00000058 R25 0x01010019 R26 0xAFA8001A R27 0x100000BB R28 0x0020011C R29 0x000000BD R30 0x0100003E