Hello everyone
I have lmk04821 eval board and I tried to run the board with using code loader on windows 7 but I get "Runtime error ' 6 ' overflow " error . How can I run code loader on windows 7 machine
Thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone
I have lmk04821 eval board and I tried to run the board with using code loader on windows 7 but I get "Runtime error ' 6 ' overflow " error . How can I run code loader on windows 7 machine
Thanks in advance
I set the decimal point period and I dont get any error thank you Timothy but I have another problem.
I connect Vcc(SMA) port to 5 volt
I connect CLKin1 to signal generator which give 122.88 MHz 0 dBm signal
I connect the eval board to PC via USB2ANY adapter
I open codeloader administration mode and select LMK04821
But I could not get any output signal from DCLKOut0 which is shown 491.52 MHz in codeloader's CLKouts sides.
How can I gen output signal from output ports
Thanks in advance