The datasheet for the LMK04906 (p.16) writes that the LEuWire pin should be set to low after programming is complete. Normally, when using an active low LE signal, we set the LE high when not programming to be sure that data isn't inadvertently written to the device. Is there a reason why the LE signal must be set low after programming? Is there any issue if the LE signal is left high after programming is complete?
Thanks.
Mark