Other Parts Discussed in Thread: CDCLVP1204
Arvind, being solved the previous issue about a CDC1204 application i would like to ask you about another one.
We are involved in a new design of an auxiliary module managing sinc signals of 1Hz (1pps) and 10 MHz), that will be auxiliar via DPLL to the main system clock.
Both signals are in digital format LV3.3V originally single ended.
We need some functions as demultiplexer/switch (dual input/one output), mux (one input/2 or 3 outputs) and so on.
I am considering the use of the CDC1204 for the use as demux, being able to select one of two inputs.
My doubt is about the use of the chip, and in general of the LVPECL, for frequencies as low as 1Hz. The reason is that this is the frequency of the pulse but we need to have the fastest rise time as possible. the output of this system is directed to a DPLL that will geerate the system clock and so it is very important for jitter concerns not to add jitter either to the 10 Mhz and to the 1pps signals. Being the 1pps signal positive pulses once every second, but with very fast rise time, i guess that I can use these technology at leats working with signals DC coupled and limitig their swing to 3.3V, is it correct? As the duty cycle uses to be small, the only "special" thing of the signal is that it stays near one second each period at 0V.
Thanks in advance