This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Maximum delay value of LMK04906

Other Parts Discussed in Thread: LMK04906

Hi,

The datasheet of LMK04906 specifies the maximum adjustable delay is 522 distribution path clock :

"Clock outputs may be delayed or advanced from one another by up to 517.5 clock distribution path periods. By programming a digital delay value from 4.5 to 522 clock distribution path periods, a relative clock output delay from 0 to 517.5 periods is achieved"

The distribution path clock can be directly bypassed from VCO, or can be the divided version of VCO, the VCO divider range is from 2~8.

Also, the VCO tuning range is from 2370 to 2600 MHz.

So, is the maximum adjustable delay value equals to 522 x 8 / 2370MHz = 1.762 us ?

In my application, I need to delay a 1MHz clock up to a full period (1 us), thanks.