This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

For TLC2932AIPWR

Other Parts Discussed in Thread: TLC2932A, CDC7005, CDCM7005

Questions about TLC2932AIPWR

1,
Frequency that can be output from VCOOUT how about you 11MHz ~ 50MHz?
(SELECT pin is "H")

2,
FIN-A, FIN-B, is about the relationship of VCOOUT.
And the FIN-A⇒1.536MHz, if you expect a VCOOUT⇒12.288MHz, Are you entering the FIN-B⇒VCOOUT ÷ 8?

3,
Case 2, the recognition is correct.
The following N to be input to FIN-B, I think no problem to be larger to infinity?
FIN-B⇒VCOOUT ÷ N
For example, what no problem even N = 2000?

Best Regards,

Kozo