Other Parts Discussed in Thread: CODELOADER
Hi,
We would like to use an external pin to FSK modulate.
Per the data sheet, this modulating pin (one of Trig_1, Trig_2, Mod) should be set to trigger TRIG_A or TRIG_B (let's assume we chose Trig_1 to activate TRIG_A), and then the device should be configured such that an FSK deviation will be activated when TRIG_A is active.
The issue that I see is that per the data sheet, TRIG_A is activated by a transition in Trig_1 (can be configured to a rising or a falling edge - let's assume rising edge).
So, the FSK deviation is applied by a rising edge in Trig_1, but I'm not sure that it is de-applied when Trig_1 goes back to zero (as I would accept from an FSK modulator).
In other words, we would like the FSK modulation to be level activated and not edge activated. Is this possible?
Thanks,