Other Parts Discussed in Thread: CDCE913, CLOCKPRO, PCA9306
Hello,
we have issues while programming CDCE913 onboard. We use 913PERF board and ClockPro software. According to the datasheet for 913PERF we connect SDA and SCL lines to our board's dedicated header.
The SDA and SCL lines are pulled up on our board to 3.3V through a 3.3k resistors. We have a CPU on this I2C bus to control CDCE913. The CPU is also clocked via CDCE913, so there is not possible to program the CDCE913 initially via CPU, we use 913PERF instead for first launch.
One year ago we build a few prototypes, all works fine, But now we cannot access the CDCE913.
The setup is only working with disconnected 3.3v pullup (high level is done via 10k pullup to 1.8V on 913PERF). Also replacing the old 3.3k to something like 43k helps but the rising edge timing is very bad in this case.
The CDCE913 datasheet says that the I2C pins are 3.3V-tolerant. What can be a cause of the issue otherwise?