This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are evaluating LMK04133EVAL by using USB2ANY with reference to snlu099A. However, even if pressing 'Ctrl - L', outputs are mute.
Input:122.88MHz/CLKin0*
Output:122.88MHz/CLKout0
Mode select of code loader:122.88MHz VCXO Default
LMK04133EVAL/EVM Ver:1111-05
*write Register
R7 (INIT) 0x00000017
R0 0x01030400
R1 0x01080101
R2 0x01080102
R3 0x01080103
R4 0x01000104
R7 0x00000007
R10 0x2150000A
R11 0x00650DEB
R12 0xE078078C
R13 0x0A04000D
R14 0x0F77002E
R15 0x1C80010F
Is there a place to be confirmed something? I have attached the setting file of code loader.
Best Regards,
Kato
Hi,
Allow me to notify you of the additional information.About evaluating LMK04133EVAL by using USB2ANY, when USB2ANY uWire pins directly were connected to LMK04133(*R12,R19 and R29 were changed to 0ohm), output frequency was mute. however, After we used these resisters, R12,R19 and R29 those were for voltage translation, output frequency was as expected. Were these registers essential for low pass filter ?
Best Regards,
Kato
Hi Alan -san,
Thank you for the reply. Our customer is evaluating LMK04133 without USB2ANY. Then, they couldn't get the expected output frequencies.
One of the differences USB2ANY signals and FPGA ones, FPGA LE signal is toggled LOW to HIGH to LOW before first set R7(INIT).
R7 (INIT) 0x00000017
R0 0x01030400
R1 0x01080101
R2 0x01080102
R3 0x01080103
R4 0x01000104
R7 0x00000007
R10 0x2150000A
R11 0x00650DEB
R12 0xE078078C
R13 0x0A04000D
R14 0x0F77002E
R15 0x1C80010F
Is this a problem? And could we discuss offline? If it is okay, could you please send me an email.?
Best Regards,
Kato
Kato-san,
It appears the used CodeLoader to generate/export the register settings.
Can you please ask them to send the CodeLoader setup file (.mac file) used to generate the register settings? This way I can load the GUI settings and graphically see their configuration details like CLKin frequency, VCXO frequency, and output frequencies, in addition to their register settings.
Thanks,
Alan
Hi Alan -san,
I would like to send you customer data. So, could you agree to my friendship request ?
Best Regards,
Kato