Hi,
I am trying to promote our clocking solution at one of my customer who does optical back hauls based on SONET standard.
The situation is that the reference clock comes from the port and we need to clean it and generate 2 frequencies mainly: 156.25 MHz (Ethernet) and 155.52 MHz (SONET) with less than 1ps jitter. There should be a flexibility to generate both the values on one output pair. That is to say, the user must be able to choose between Ethernet and SONET clock on the same line by changing the output divider setting.The most important thing is the hold-over option. The output frequency must be held in spite of the absence of the reference input .
I checked LMK04808, LMK04906 as they has hold-over but it lacks fractional divider required to generate both the frequencies on the same line.
Do we have any solution for this?