Other Parts Discussed in Thread: LMK04906, CODELOADER, LMK04828
Hi,
Could you please suggest the appropriate product to us as following requirements from the jitter cleaner solution ?
Is our understanding correct although we will try to suggest LMK04906 to our customer ?
In addition, could you please tell us how to configure LMK04906 and share the sample schematic including the external components if it is correct ?
<Requirements>
Clock Input Frequency Range : 10MHz ~ 50MHz
Clock Output Frequency Range : 10MHz ~ 50MHz
Ratio of Output to Input Frequency : 1[MHz/MHz](0dB)
Input Level : LVCMOS
Output Level : LVCMOS
Best regards,
Kato