This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
I am a student from Nanyang Technologinal University.
Now i am testing the LMX2492 Eval Board. I downloaded and installed the current version of CodeLoader.
I followed all the instructions on LMX2492EVM User's guide.
Then i tried the example provided on page19. But i cannot get the ramp signal centered at 4.8GHz(vco/2).
The signal i got on spectrum analyzer is attached. Screenshots of other configurations are also provided.
Is there anything else i forgot to do?
Thanks!~
Hi zhixiang,
Thank you for your interest in our products. We received your question and will be answering it as soon as possible. We appreciate your patience.
Regards,
Julian
I don't see anything wrong with this setup. However, to get the ramping to start, you ahve to toggle the RAMP_EN bit or write to the N divider.
Coudl this be the issue?
I also assume that you have tested that the PLL locks to the corrrect frequency.
There is a divide by 2 on teh output of the VCO on our eval board the frequency that your carrier is at does not seem to be withing the range you are ramping at all.
If you have not achieved a lock on our board, try this:
1. Use the default mode
2. Press CTL+L to lock
3. If no lock, try toggling the POWERDOWN bit to ensure that the current is changing. If not, then perhaps there is a communication issue with the device.
REgards,
Dean
Regards,
Dean