Other Parts Discussed in Thread: LMX2582, LMX2485, LMX2492
Hello,
I am working on a project where I am measuring the distance between two objects. I plan to send a signal (sine wave) from one object to the other and measure the phase difference between that signal and a base signal. Based upon this phase difference I should be able to calculate the distance the signal traveled.
In order to do this I have found that I will need to measure the phase difference between a 3GHz, 300MHz, 30MHz, 3MHz, and 300KHz signal (Sine wave) to meet the accuracy and range requirements of my project.
I was wondering if there are any products that are capable of measuring the phase at such frequencies?
Thank you,
-Erik Juziuk