Other Parts Discussed in Thread: LMX2592
Is there a way to manually tune the VCO inside the LMX2592? Also, can the band/capacitor values be read after an internal calibration to a desired frequency?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMX2592
Is there a way to manually tune the VCO inside the LMX2592? Also, can the band/capacitor values be read after an internal calibration to a desired frequency?
Gary,
Yes, so first do a normal calibration to the desired frequency, then tristate the charge pump (register CP_EN=0). Then you can tune the voltage at Vtune (device pin 35) between 0 and 2.5V to adjust the VCO manually. There is readback for register values but not for actual internal component values. Thanks!
Regards,
Brian Wang