This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.i need the design files/bom for timing circuit for our controller.The se555m should work great.6 to 12 second variable on time monostable driving n channel mosfet for relay coil with 65ma min current draw.Any help greatly appreciated.Need for gerbers.Can not use sink capabilities due to current design with external timers.smd/smt required for 2 layer pcb.
Hi,
I have forwarded your query to the applications engineer most familiar with this part. Expect a reply soon.
Regards
Arvind Sridhar
Hi Ron.We have an award winnining automotive aftermarket product from the 2015 sema convention in Las Vegas.The controller may have to to potted if installed under the hood.We really dont want to do thjis.Toyota is interested in this as a oem part for the trucks.The current timers we use are the pac tr7 programable.type which get neg. trigger pulse from door actuators.but they are externally under dash.We want to put them on the pcb of exhisting design.I think automotive temp rateing is what we have to go with.We can vary timing with pot.for calibration.We have a manufacturer working on revision of mechanical side.We need your input so we can get pcbs into production ASAP.I have a pcb designer who can run with your schematic and bom and genrerate gerber files.Very possable we will be purchasing large quanty of o you bom.as soon as prototype testing completed.
Thank You
Bob Kirk
Step-Lock inc.
602-796-9485
Hi Ron,Sorry just not available until 4:30.I looked at figure 9.Its pretty straight forward,Maybe 500k pot would work for calibration of timer.Is pull up on output necessary if driveing mosfet gate..Can you recommend a mosfet.N channel 1 amp 12.6 volt/.The load dump is not an issue as the controller is only powerd when key is off.No altenator voltage.What about gate capacitance.Logic level mosfet would be fully on with 12vdc right.Trigger is from door actuator.neg pulse.Is discrimenator needed.