This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2592 time auto calibration 22 us. Under what conditions can be achieved.

Other Parts Discussed in Thread: LMX2592, LMX2592EVM, LMX2582

Hi All.

When working with LMX2592EVM I can not achieve in a given time auto calibration in datasheet LMX2592 (p.31) about 22us.
We achieve time auto calibration for at least 2 ms.

The parameters of the PLL:
mode - FRAC, Fpfd = 200 MHz, Ref in = 200 MHz, R = 1,
ACAL_FAST = 1, FCAL_FAST = 1, CAL_CLK_DIV = 0.

Other parameters LMX2592, such as spectral content, phase noise, spurs, we have measured and have no questions.
Question - only one: under what conditions can be achieved auto-calibration time about 22us.

Thanks.