Other Parts Discussed in Thread: LMX2592
Hi Support,
Based on the PLLatinum Sim, the total lock time=VCO calibration time + Analog lock time from Start freq F1 to Stop freq F2.
1) Is there any latency involved in the total lock time above that is not stated? E.g. PLL SPI command decoding time
2) Do you have a timing diagram (start to stop with timing values) to show the entire sequential process involved when command is sent from FPGA to LMX2592 to change freq from F1 to F2 till final F2 lock time, assuming external clock is 100MHz?
Thanks.