Other Parts Discussed in Thread: CDCE913
I've got a CDCE913 on a board nearing production that I need to write the EEPROM on (so it starts in power-down mode to limit power-on surge current). The problem is, nothing happens when I set EEWRITE to 1. EEPIP never changes, and a power-cycle of the chip brings back the same old default configuration.
I've confirmed that I2C is behaving properly, the byte write I do to set register 2 to 0x00 (power-down) works, and the bus cycle to set register 6 to any value with bit 0 (EEWRITE) set looks exactly the same, ACK and all. But nothing ever actually happens.
I need to find a solution to this soon...