LMX2592
TI engineer,
What kind of waveform can I expect at the output of the LMX2592 synthesizer? From the EVM board I measured more of a square wave at 930MHz on output A. Output B looks more like a sinusoidal but is still not perfect (I figure the filter toke out some harmonics). I also used the onboard oscillator. I would like a sinusoidal wave at 930Mhz and possibly at 2.4 GHz (ISM band). The power output isn't that important and the application doesn't require any fast switching speeds. Is this possible or will I have to filter out what I don't want?
Secondly, I would like to use the EVM part layout for my board but have to make a few modifications. It would be unpleasant to come up with my own Altium Designer/Eagle design/layout. Would it be possible to send the needed files (Gerber, .docPCB, etc.)?
Thank you,
Brandon Becker