Other Parts Discussed in Thread: CDCM61004, CDCM6100XEVM
Hi,
I will use the CDCM61004 in my design. For my circuit design I looked at eval board circuit of the CDCM6100xEVM. In this circuit I do not understand why a 10pF capacitor parallel to the crystal is required. Do I need a capacitor when I use a crystal with 10pF load capacity?
Next question is the connection of a LVCMOS oscillator. Do you recommend a 3,3V dc coupled device or a 2,5V ac coupled LVCMOS in order to achieve low jitter and high accuracy?
Thanks!
Best regards from Austria,
Daniel