I've been evaluating the LMK61E2 and while the phase noise meets my project requirements, the stability does not. Is there any chance that this device might be available (someday) with an high stability external reference (50 MHz OK but 10 MHz better)? Or - - - does TI have another device in a similar "crystal" type package, which has the phase noise of the LMK61E2 but also has the external reference capability? I searched but nothing jumped out....Thanks Bill