This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL5010 as 10 Minute Timer

Other Parts Discussed in Thread: TPL5010

Hi,

i need a setup for the TPL5010 as 10 Minute Timer.

I have only 1 Pin on my µC as Interrupt/Wakeup pin.

So After 10 min the Interrupt Pin should go from HIGH to LOW.

  • Please stand by, I've notified the appropriate engineer.
  • Hi Stephan.

    If you have just one pin available for interrupt and wake up it means that you are not interested to the watchdog feature isn't it ?

    If so you can use the Reset pin of the TPL5010 to wake up your uC. Make sure to connect the DONE pin to GND and leave the WAKE floating . Connect the RESET pin of the TPL5010 to the interrupt pin of your  uC  and do not forget the pull-up resistance.

    In the Datasheet you can find the right value of the external eresistancee to set 10 min.

    Regards Domenico