Other Parts Discussed in Thread: LMK04828, ADC12J4000, LMX2582, LMX2541
Hi,
I'm starting to develop a module that incorporate an ADC (JESD204 inteface), FPGA DAC & need a clocking solution.
I wish to use the LMK04828 with a 100MHz input clock to drive the FPGA & ADC12J4000.
The required sampling frequency is 2.7GHz.
I see that the LMK04828B VCO does not support this frequency:
2370 to 2630 MHz & 2920 to 3080 MHz.
Is that correct?
Do you have any suggestion as to how to overcome this limitation?
Regards,
Itai