Other Parts Discussed in Thread: LMK00804B
Dear all,
Can LMK00804B support 50MHz 20% duty cycle input clock? If yes, how about the additive jitter and the duty cycle of single-ended LVCMOS output clock?
Input of LMK00804B: 50 MHz 20% duty cycle LVDS clock to CLK/nCLK pins with Slew Rate more than 3V/ns.
Power Supply of LMK00804B: Core supply is 3.3V; Output supply is 1.5V.
Thanks in advance.
Regards,
Minglei