Hello,
I am currently working on a CDCM6208V2 Evaluation Board.
I use the GUI to configure my chip.
My configuration is the following:
SECp = crystal input 10 MHz
M = 125
N = 6250
f_PFD = 80 kHz
Loop Filter = configuration 4 (p.16 Evaluation Board datasheet)
f_VCO = 3000 MHz
PSA = 6
PSB = 6
PRE = 2
FRA = 122.0703125
Y4 = LVCMOS 2.048 MHz, 0 PPM
As you can see I should obtain 2.048 MHz on Y4 but I measure 1.93113 MHz (about 5.71% error).
I also tried to use Y0 with an integer divider of 50 (Y0 LVPECL output 10 MHz) to test the accuracy but I measure 9.4337 MHz (also about 5.71% error).
I would like to know where this error comes from. (VCO frequency?).
Also I am forced to put 2.171943 MHz for Y5 on the GUI (PRE = 2, FRA = 115.1043176) to measure 2.048 MHz in output.
This method to get the frequency I want in output bothers me a little bit.
Thank you for your help,
Simon