CDCM6208 datasheet written about input/output duty cycle below.
・Page 9 :IDC (Deference Input Duty Cycle) ⇒ 40%~60%
・Page 12:ODC (Output Duty Cycle) ⇒ 45%~55%
If custoer's input duty cycle is narrow range (48%~52%), will output duty cycle be narrow range, too?
If correct, is output duty cycle less than 48%~52% or more narrow?
Best regards,
Satoshi