Other Parts Discussed in Thread: CDCE62002EVM
Hi,
I am using CDCE62002 as a cleaner for 960MHz. and 80MHz clock, and using a 20MHz crystal.
The parameters I am using are(generate by theCDCE62002 EVM ):
Register 0: 0x660810A0
Register 1: 0x83856001
Register 2: 0x00000002
When I write and read the registers, it has a proplem. After I write the registers and begin to read the registers, I can read the parameters in register 0 right, but the parameters in register 1 is wrong. I checked the Timing Diagram of my progrom, and I didnot find anything wrong. So, I am confused now.
Need your help!
Best regards
Kun Zhang