This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2571: unused pin



Hi all, 
Could you please tell me how to handle below unused pins?

FSKDx:        
OSC*:           When Single end configuration 
TrCtl:            When RXTX_CTRL=0
FLout1/2:
CPoutExt:    When the external VCO is not used
RFoutTx:     

Thanks in advance.
Regards,
Toshi

  • Hi Toshi,

    if you do not use FSK Pin mode or FSK I2S mode, you can leave FSK_Dx pins floating.
    OSCin* could be left floating for single-ended input.
    TrCtl, FLout1/2, CPoutExt can be left floating if you do not use them.
    RFoutTx, if your configuration is push-pull output, leave it floating if not being used.