I have already seen in datasheet that DCORSELx, DCOx and MODx are configurable to choose a DCO frequency range, but I would like to know if I don't configure it in code which range is the default. I believe it is 0.32 to 0.75 MHz, am I right?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have already seen in datasheet that DCORSELx, DCOx and MODx are configurable to choose a DCO frequency range, but I would like to know if I don't configure it in code which range is the default. I believe it is 0.32 to 0.75 MHz, am I right?
Hi Sara,
Please re-post in the MSP430 forum: 
Best Regards,
Julian