Other Parts Discussed in Thread: CDCE72010, ADS62P49
Hello,
J'd like to clock the TI ADC ADS62P49 with a frequency of 250 MHz clock with low jitter. Therefor I use the CDCE72010 chip with an 250 MHz VCXO and an 25 MHz reference oscillator.
I' ve read the whole datasheet but have still one question:
The Output-Register-Bits from 6 to 12 (PH#ADJC#) are to select the "Coarse Phase adjust" for each output channel. But where can I find the table with values I have to write to this register-bits? In the datasheet, page 59, stands: For a complete listing of the coarse phase adjust settings, refer to the CDCE72010 Coarse Phase Adjust" document. But I cant find this document...
I' d like to set the output divider to 1 and 0 degree phase shifting...
Refer to page 34 of the datasheet, to set output divider to 1, I have to write 0100000 in the Output Register Bit 13 - 19. In this table stands, that with divider 1 the phase shifting is 0 degree.... but why are there extra PH#ADJC# Bits???
Regards Simon