Other Parts Discussed in Thread: LMK04826
Hi,
I'm using the LMK04826 with a single ended 10MHz sine wave for the PLL2 reference input, OSCin. This violates the datasheet minimum slew rate of 0.15V/ns. It has been working with no issues on a custom board. The footnote (2) in the datasheet mentions that the jitter performance will go down as the slew rate is decreased. Is it ok to operate below the minimum if I can tolerate the decrease in jitter performance? Will the PLL shut off or lose lock over temperature, or experience any other problems? Or has it just not been characterized below the minimum listed?
Thanks.