This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[ LMX2582 ] Post-R Divider Frequency Range

Other Parts Discussed in Thread: LMX2592

[ LMX2582 ] Post-R Divider Frequency Range

Hi,

Can you help me to understand frequency range of Post-R Divider?
According to datasheet, Post-R Divider should be used when extended PFD mode enabled. This means PFD can support from 250KHz to 400MHz.



However, table 1 says that the output frequency range is from 0.25  to 125MHz.
Can you explain how I understand this Output high frequency?

The datasheet of LMX2592 describe same information, too.

Thanks,
Ken