Hello Everyone,
If anyone has tried out block read for register readout of CDCE913 PLL chip.
I cannot get it work.
My situation is: the byte write, byte read and block write are OK, meaning i2c works fine (SCL 11kHz).
I take the programing sequence suggested by Datasheet (page12) also for block read
but whatever byte offset i set, the data i read out is always FF.
The diagnostic showed that CDCE913 in the 4th step of the sequence -readout of byte count- gives the correct block count as set previously in BCOUNT register. This means the block read command is correctly interpreted by CDCE913, but the data read out always gives FF.
If it is a software problem, the only possiblilty is that the byte offset (in CommandCode) is wrong, but i'm sure the code for CommandCode setting is identical to byte write, byte read and block write.
So my guess is that there is an error in data sheet (revised oct 2009) or in silicon.
Although it is harmlos to use byte read instead of block read, but i still appreciate any answer.
Thanks in advance