Is there a minimum resistance requirement for the TLC-555 RC Time Constant input(s)? I reviewed the datasheet and could not find a specification.
With the 74LS121 there is a minimum resistance requirement of 1400 Ohm for the RC Time Constant. Is there a similar minimum resistance requirement for the TLC-555
Below is a schematic of the One Shot circuit I am working on. The question revolves around the Resistance Value of "R3" (2.2k Ohm) which is to allow the RC Time Constant to always have "some" resistance if VR1 value is turned down to 0 Ohms (20K Ohm Variable Resistor).
I just don't know what the minimum resistance for "R3" can be. I would like to know the minimum allowable resistance for "R3" without damaging the TLC-555.
Note: C6 & C7 are mounted as physically close to pins 4 & 8 as possible.
Thanks,
Rhode