Hi,
I have a question about LMK04906 clock output format.
I need five 80MHz LVCMOS output and four 26+2/3MHz LVCMOS output, total 9 LVCMOS outputs.
Also I want all LVCMOS outputs to be same polarity, so that I guess appropriate format is LVCMOS(Norm/Norm).
In LMK04906 datasheet page.111 "9.4.1 LVCMOS Complementary vs Non-Complementary Operation",
it said as follow:
*************************************************************************
A non-complimentary format such as LVCMOS (Norm/Norm) is not recommended
as increased switching noise is present.
*************************************************************************
Does this mean that I should not select LVCMOS(Norm/Norm) and
same polarity of 9 LVCMOS output are not available for LMK04906?
Are there any method to realize 9 LVCMOS output with same polarity?
best regards,
g.f.