I'd like to use the TPL5110 as a power-on controller, to hold a larger system in power-down until a momentary pushbutton is pressed. One question is this: it looks from the datasheet that if the DELAY/M_DRV signal is held high with EN/ONE_SHOT held low, the DRV output will remain low. Is that actually the case? If M_DRV is held high, DRV will he held low, and then when M_DRV is released, DRV will be driven high after a time determined by the resistor on M_DRV? And, after all of this, the one-shot functionality will be re-enabled for subsequent button presses?