This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ds64br111 does not transmit first bit

Other Parts Discussed in Thread: DS64BR111

Hi all,

my customer is using 2 SATA channels (6Gbps), each channel has 2 DS64BR111, one close to Transmitter board and another close to the receiver board.

He has selected for the AC coupling 220nF capacitance. The devices have been configured in slow OOB. One channel works very well, while the other one with the same schematic does not.

From the scope the deisgner has seen that the first bit of the SATA protocol is not sent. 

Could the  different layout between the 2 channles and the high capacitance for the AC couplig increase the charging time of the caps ?

any hint ?

Thanks,

Domenico